LS1028A TFA problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1028A TFA problems

2,849 Views
barce
Contributor I

Hello, When burning the system via an SD card on my 1028A board, I encountered issues during the BL2 phase of TFA (Trusted Firmware-A). Sometimes it fails at loading image 4 during the BL2 stage, and other times it fails at loading image 5. The specific issues are as follows. How can I resolve this problem? thank you!

INFO: RCW BOOT SRC is SD

INFO: SoC workaround for DDR Errata A009803 was applied

INFO: SoC workaround for DDR Errata A009942 was applied

INFO: SoC workaround for DDR Errata A010165 was applied

INFO: time base 0 ms

NOTICE: Fixed DDR on board

INFO: Time after parsing SPD 4 ms

INFO: Time before programming controller 8 ms

NOTICE: 2 GB DDR4, 32-bit, CL=11, ECC off

INFO: Time used by DDR driver 18 ms

INFO: RCW BOOT SRC is SD

INFO: esdhc_emmc_init

INFO: Card detected successfully

INFO: init done:

NOTICE: BL2: Built : 11:17:14, Feb 28 2025

INFO: Configuring TrustZone Controller

INFO: ******* image_id: 3 ********

INFO: image_base: 4225761280;image_size: 0;image_max_size: 2097152;

INFO: type: 1;version: 2;size: 24;attr: 4

INFO: ******* image_id: 4 ********

INFO: image_base: 4227858432;image_size: 0;image_max_size: 67108864;

INFO: type: 1;version: 2;size: 24;attr: 0

INFO: ******* image_id: 5 ********

INFO: image_base: 2181038080;image_size: 0;image_max_size: 2044723200;

INFO: type: 1;version: 2;size: 24;attr: 0

INFO: BL2: Doing platform setup

NOTICE: start bl2_load_images id 3

INFO: BL2: Loading image id 3

INFO: Loading image id=3 at address 0xfbe00000

INFO: Image id=3 loaded: 0xfbe00000 - 0xfbe0d23d

INFO: load_auth_image_internal: 0

NOTICE: start post_image_load id 3

NOTICE: start bl2_load_images id 4

INFO: BL2: Loading image id 4

WARNING: Firmware Image Package header check failed. id=0

WARNING: Failed to obtain reference to image id=4 (-2)

INFO: load_auth_image_internal: -2

ERROR: BL2: Failed to load image id 4 (-2)

Authentication failure


INFO: image_base: 4225761280;image_size: 0;image_max_size: 2097152;

INFO: type: 1;version: 2;size: 24;attr: 4

INFO: ******* image_id: 4 ********

INFO: image_base: 4227858432;image_size: 0;image_max_size: 67108864;

INFO: type: 1;version: 2;size: 24;attr: 0

INFO: ******* image_id: 5 ********

INFO: image_base: 2181038080;image_size: 0;image_max_size: 2044723200;

INFO: type: 1;version: 2;size: 24;attr: 0

INFO: BL2: Doing platform setup

NOTICE: start bl2_load_images id 3

INFO: BL2: Loading image id 3

INFO: Loading image id=3 at address 0xfbe00000

INFO: Image id=3 loaded: 0xfbe00000 - 0xfbe0d23d

INFO: load_auth_image_internal: 0

NOTICE: start post_image_load id 3

NOTICE: start bl2_load_images id 4

INFO: BL2: Loading image id 4

INFO: Loading image id=4 at address 0xfc000000

INFO: Image id=4 loaded: 0xfc000000 - 0xfc07bdc0

INFO: load_auth_image_internal: 0

NOTICE: start post_image_load id 4

NOTICE: start bl2_load_images id 5

INFO: BL2: Loading image id 5

WARNING: Firmware Image Package header check failed. id=0

WARNING: Failed to obtain reference to image id=5 (-2)

INFO: load_auth_image_internal: -2

ERROR: BL2: Failed to load image id 5 (-2)

Authentication failure

 

 

Tags (1)
0 Kudos
Reply
1 Reply

2,826 Views
yipingwang
NXP TechSupport
NXP TechSupport

1. Please use QCVS DDRv tool to do DDR optimization and validation.

2. Please refer to the following document to debug ATF.

https://community.nxp.com/t5/Layerscape-Knowledge-Base/Debugging-ATF-and-u-boot-with-CodeWarrior-for...

 

0 Kudos
Reply