LS1028A / LS1027A: disabling GPU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1028A / LS1027A: disabling GPU

跳至解决方案
2,058 次查看
mbourhis
Contributor II

LS1028A and LS1027A are 2 SoC of the same family.

LS1028A has a GPU (GC7000UltraLite) and LS1027A has not.

Is it possible, through a software configuration, to disable the LS1028A GPU?

(with a modification in DeviceTree file, or a Kernel option or a Boot argument?)

 

Thanks for your help.

Regards,

 

0 项奖励
回复
1 解答
2,042 次查看
ufedor
NXP Employee
NXP Employee

GPU can be disabled by setting DEVDISR6[GPU] in PBL.

This can be done as RCW source modification by adding ".rcw" file containing:

.pbi
write 0x1e00084,0x00001000
.end

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,043 次查看
ufedor
NXP Employee
NXP Employee

GPU can be disabled by setting DEVDISR6[GPU] in PBL.

This can be done as RCW source modification by adding ".rcw" file containing:

.pbi
write 0x1e00084,0x00001000
.end

0 项奖励
回复