LS1021a-TWR PCIe linux driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021a-TWR PCIe linux driver

ソリューションへジャンプ
2,802件の閲覧回数
jasonhendrix
Contributor V

In the QorIQ SDK documentation, the Linux driver section 7.11 references the MPC85xx platform and Linux 3.19.3 or later.  Is there a pcie Linux driver for the LS1021A-TWR?

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
2,459件の閲覧回数
ufedor
NXP Employee
NXP Employee

In the SDK 1.9 Documentation (Submit Form ) it is written:

Specifications

Target board:Freescale MPC85xx/Layerscape platform and PCIe Add in Card
CPU:Freescale MPC85xx/Layerscape Processor

Here "Layerscape" corresponds to the LS1021A-TWR as well.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,460件の閲覧回数
ufedor
NXP Employee
NXP Employee

In the SDK 1.9 Documentation (Submit Form ) it is written:

Specifications

Target board:Freescale MPC85xx/Layerscape platform and PCIe Add in Card
CPU:Freescale MPC85xx/Layerscape Processor

Here "Layerscape" corresponds to the LS1021A-TWR as well.

0 件の賞賛
返信