LS1021a-TWR PCIe linux driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021a-TWR PCIe linux driver

Jump to solution
2,807 Views
jasonhendrix
Contributor V

In the QorIQ SDK documentation, the Linux driver section 7.11 references the MPC85xx platform and Linux 3.19.3 or later.  Is there a pcie Linux driver for the LS1021A-TWR?

Labels (1)
0 Kudos
Reply
1 Solution
2,464 Views
ufedor
NXP Employee
NXP Employee

In the SDK 1.9 Documentation (Submit Form ) it is written:

Specifications

Target board:Freescale MPC85xx/Layerscape platform and PCIe Add in Card
CPU:Freescale MPC85xx/Layerscape Processor

Here "Layerscape" corresponds to the LS1021A-TWR as well.

View solution in original post

0 Kudos
Reply
1 Reply
2,465 Views
ufedor
NXP Employee
NXP Employee

In the SDK 1.9 Documentation (Submit Form ) it is written:

Specifications

Target board:Freescale MPC85xx/Layerscape platform and PCIe Add in Card
CPU:Freescale MPC85xx/Layerscape Processor

Here "Layerscape" corresponds to the LS1021A-TWR as well.

0 Kudos
Reply