LS1021ATWR SDK2, Linux-4.1.8-rt8+gbd51baf, udevd timeout, no usb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021ATWR SDK2, Linux-4.1.8-rt8+gbd51baf, udevd timeout, no usb

Jump to solution
1,894 Views
xkonni
Contributor II

running the kernel, dtb, rootfs included in the sdk2, in addition to network issues - see other thread - i can not use any usb devices. the usb subsystem seems to die on boot. please see the attached log.

 

thanks for your help,

 

Konstantin

Original Attachment has been moved to: uboot-usb.log.zip

Labels (1)
0 Kudos
Reply
1 Solution
1,721 Views
xkonni
Contributor II

forgot to post this here.

just like with the networking issue, using the new u-boot fixed it.

thanks for your help!

View solution in original post

0 Kudos
Reply
2 Replies
1,721 Views
Pavel
NXP Employee
NXP Employee

Your dump shows that there is no connection to USB device.

Test your board using different USB port of the LS1021ATWR board.

Test your board using different USB device (USB Flash).

Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,722 Views
xkonni
Contributor II

forgot to post this here.

just like with the networking issue, using the new u-boot fixed it.

thanks for your help!

0 Kudos
Reply