LS1021ATWR SDK2, Linux-4.1.8-rt8+gbd51baf, udevd timeout, no usb

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1021ATWR SDK2, Linux-4.1.8-rt8+gbd51baf, udevd timeout, no usb

跳至解决方案
1,819 次查看
xkonni
Contributor II

running the kernel, dtb, rootfs included in the sdk2, in addition to network issues - see other thread - i can not use any usb devices. the usb subsystem seems to die on boot. please see the attached log.

 

thanks for your help,

 

Konstantin

Original Attachment has been moved to: uboot-usb.log.zip

标签 (1)
0 项奖励
回复
1 解答
1,646 次查看
xkonni
Contributor II

forgot to post this here.

just like with the networking issue, using the new u-boot fixed it.

thanks for your help!

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,646 次查看
Pavel
NXP Employee
NXP Employee

Your dump shows that there is no connection to USB device.

Test your board using different USB port of the LS1021ATWR board.

Test your board using different USB device (USB Flash).

Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,647 次查看
xkonni
Contributor II

forgot to post this here.

just like with the networking issue, using the new u-boot fixed it.

thanks for your help!

0 项奖励
回复