LS1021ATWR SDK2, Linux-4.1.8-rt8+gbd51baf, udevd timeout, no usb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021ATWR SDK2, Linux-4.1.8-rt8+gbd51baf, udevd timeout, no usb

ソリューションへジャンプ
1,812件の閲覧回数
xkonni
Contributor II

running the kernel, dtb, rootfs included in the sdk2, in addition to network issues - see other thread - i can not use any usb devices. the usb subsystem seems to die on boot. please see the attached log.

 

thanks for your help,

 

Konstantin

Original Attachment has been moved to: uboot-usb.log.zip

ラベル(1)
0 件の賞賛
返信
1 解決策
1,639件の閲覧回数
xkonni
Contributor II

forgot to post this here.

just like with the networking issue, using the new u-boot fixed it.

thanks for your help!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,639件の閲覧回数
Pavel
NXP Employee
NXP Employee

Your dump shows that there is no connection to USB device.

Test your board using different USB port of the LS1021ATWR board.

Test your board using different USB device (USB Flash).

Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,640件の閲覧回数
xkonni
Contributor II

forgot to post this here.

just like with the networking issue, using the new u-boot fixed it.

thanks for your help!

0 件の賞賛
返信