LS1021A v2.0 - microcode version

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1021A v2.0 - microcode version

跳至解决方案
2,824 次查看
Davisg
Contributor III

Is the following the correct microcode version for the LS1021A v2.0?

CPU:   Freescale LayerScape LS1021, Version: 2.0, (0x87001120)

.

.

.

Firmware 'Microcode version 0.0.1 for LS1021a r1.0' for 1021 V1.0

QE: uploading microcode 'Microcode for LS1021a r1.0' version 0.0.1

标签 (1)
0 项奖励
回复
1 解答
2,609 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,


yes, this message shows the correct microcode version for the LS1021A v2.0

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,610 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,


yes, this message shows the correct microcode version for the LS1021A v2.0

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复