LS1021A v2.0 - microcode version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021A v2.0 - microcode version

Jump to solution
2,837 Views
Davisg
Contributor III

Is the following the correct microcode version for the LS1021A v2.0?

CPU:   Freescale LayerScape LS1021, Version: 2.0, (0x87001120)

.

.

.

Firmware 'Microcode version 0.0.1 for LS1021a r1.0' for 1021 V1.0

QE: uploading microcode 'Microcode for LS1021a r1.0' version 0.0.1

Labels (1)
0 Kudos
Reply
1 Solution
2,622 Views
r8070z
NXP Employee
NXP Employee


Have a great day,


yes, this message shows the correct microcode version for the LS1021A v2.0

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,623 Views
r8070z
NXP Employee
NXP Employee


Have a great day,


yes, this message shows the correct microcode version for the LS1021A v2.0

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply