LS1021A pull-down on GPIO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021A pull-down on GPIO

2,150 Views
amin_altabich
Contributor II

We would like to ensure low status on reset of GPIO1_16 on LS1021A which is initially open and stays high after the OS boot. Currently, the pin stays high on reset. The question is, can this pin be pulled down (33k ohm) to force low on reset? Manual says "When programmed as an output, no termination is required". What method would you suggest?

Labels (1)
0 Kudos
Reply
2 Replies

2,055 Views
amin_altabich
Contributor II

Thank you. We also noticed that pull-down through 75k+ ohm resistor doesn't set the pin to low. Hence, we are expecting there is an internal pull-up on GPIO pins, with a value somewhere around 1M ohm. Is that correct? Could you give us an exact value of that pull-up?

0 Kudos
Reply

2,055 Views
ufedor
NXP Employee
NXP Employee

> The question is, can this pin be pulled down (33k ohm) to force low on reset?

Yes.

When PORESET_B is asserted GPIO signal is tri-stated.

After reset GPIO signal is configured as input.