LS1021 EDMA single request in u-boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1021 EDMA single request in u-boot

1,847 次查看
ivanpetrov
Contributor II

Hello.

I am trying to perform a single mem to mem copy in u-boot via edma. Here is my setup for TCD_#0:

int ch = 0;
out_be16(EDMA_BASE + EDMA_TCD_CSR(ch), 0x0);
out_be16(EDMA_BASE + EDMA_TCD_CITER(ch), 0x0);
out_be16(EDMA_BASE + EDMA_TCD_BITER(ch), 0x0);
out_be32(EDMA_BASE + EDMA_TCD_SADDR(ch), 0xA0000000);
out_be32(EDMA_BASE + EDMA_TCD_DADDR(ch), 0xA1000000);
out_be16(EDMA_BASE + EDMA_TCD_ATTR(ch), 0x202);
out_be16(EDMA_BASE + EDMA_TCD_SOFF(ch), 0x4);
out_be32(EDMA_BASE + EDMA_TCD_NBYTES(ch), 1024);
out_be32(EDMA_BASE + EDMA_TCD_SLAST(ch), 0);
out_be16(EDMA_BASE + EDMA_TCD_DOFF(ch), 0x4);
out_be16(EDMA_BASE + EDMA_TCD_CITER(ch), 0x1);
out_be16(EDMA_BASE + EDMA_TCD_BITER(ch), 0x1);
out_be32(EDMA_BASE + EDMA_TCD_DLAST_SGA(ch), 0);

out_be16(EDMA_BASE + EDMA_TCD_CSR(ch), 0x1);

What I was trying to achieve is having 1024 bytes copied from 0xA0000000 to 0xA1000000 in one edma major loop triggered via software. Unfortunately, that didn't work. Nothing was copied and I got an error in DMA_ES (VLD=1; DOE=1; NCE=1), which made no sense to me. And I've also noticed that writing 0x1 to BITER has no effect, as it reads back 0x0.

Is there anything wrong with my setup?

How am I supposed to set CITER=BITER=0x1?

标签 (1)
标记 (4)
0 项奖励
回复
1 回复

1,777 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached eDMA  test example for OCRAM to OCRAM transactions.

0 项奖励
回复