LS1021A - USB 3.0 controller as USB 2.0 problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1021A - USB 3.0 controller as USB 2.0 problem

3,286 次查看
hwei
Contributor III

Hi,

I have a question about the USB3.0 controller.

Can I just connect the USB2.0 part (just USB1_D_M/P)of the USB3.0 PHYs and treat the USB3.0 controller as an USB2.0 one? Is it a possible/right method?

We follow did some design like this and it seems the USB3.0 controller cannot work properly. Do I need any special setting to make it work as an USB2.0 controller?

It prompts:

usb 1-1: new high-speed USB device number 2 using xhci-hcd

usb 1-1: Device not responding to set address.

usb 1-1: Device not responding to set address.

usb 1-1: device not accepting address 2, error -71

usb 1-1: new high-speed USB device number 3 using xhci-hcd

usb 1-1: Device not responding to set address.

usb 1-1: Device not responding to set address.

usb 1-1: device not accepting address 3, error -71

...

Thanks.

标签 (1)
标记 (1)
3 回复数

2,578 次查看
ufedor
NXP Employee
NXP Employee

> We follow this and it seems the USB3.0 controller cannot work properly.

What you have done?

What are the results?

Is USB_GHWPARAMS3[DWC_USB3_SSPHY_INTERFACE]=0? (to disable the USB3 PHY)

0 项奖励
回复

2,578 次查看
hwei
Contributor III

Hi ufedor,

Do I need some specific software settings? Should I use usb2.0 driver instead of the default usb3.0 driver?

I found there is something like "usb 2.0 only mode" in RM, but I cannot find any details.

The error from kernel log:

usb 1-1: new high-speed USB device number 2 using xhci-hcd

usb 1-1: Device not responding to set address.

usb 1-1: Device not responding to set address.

usb 1-1: device not accepting address 2, error -71

I tried to set USB_GHWPARAMS3[DWC_USB3_SSPHY_INTERFACE] to 0 but it didn't change. Should I change some extra register?

Thanks.

0 项奖励
回复

2,578 次查看
ufedor
NXP Employee
NXP Employee

Could you please check whether a USB 3.0 device is properly recognized in your system?

0 项奖励
回复