[LS1021A TWR] external trigger signal for ETSEC.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[LS1021A TWR] external trigger signal for ETSEC.

跳至解决方案
949 次查看
devasish
Contributor I

I am using an LS1021A-TWR board and need to provide 1 PPS external trigger signal. 

Referred to 8.7.7.2 External trigger signal from LSSDK 21.08, but I am still not getting the data in fifo. It talks about proper RCW settings to enable this. This is RCW from the bootup logs from the device:

 

Reset Configuration Word (RCW):
       00000000: 0608000c 00000000 00000000 00000000
       00000010: 30000000 00007900 60040a00 21046000
       00000020: 00000000 00000000 00000000 18000000
       00000030: 00080000 891b7340 00000000 00000000

 

Can someone please confirm if this is correct. If not what should be the correct RCW configuration and how to update the same. 

Thanks

0 项奖励
回复
1 解答
922 次查看
khushbur
NXP TechSupport
NXP TechSupport

Hi @devasish 

Please refer to the following bit 422-424 in LS1021 Referance Manual section 4.4.6.1 RCW field definitions, please refer to 010 option.

Please follow QCVS_PBL_User_Guide to set RCW parameter according to your requirement.

 

Thanks

Khushbu Patel

在原帖中查看解决方案

1 回复
923 次查看
khushbur
NXP TechSupport
NXP TechSupport

Hi @devasish 

Please refer to the following bit 422-424 in LS1021 Referance Manual section 4.4.6.1 RCW field definitions, please refer to 010 option.

Please follow QCVS_PBL_User_Guide to set RCW parameter according to your requirement.

 

Thanks

Khushbu Patel