I am using an LS1021A-TWR board and need to provide 1 PPS external trigger signal.
Referred to 8.7.7.2 External trigger signal from LSSDK 21.08, but I am still not getting the data in fifo. It talks about proper RCW settings to enable this. This is RCW from the bootup logs from the device:
Reset Configuration Word (RCW):
00000000: 0608000c 00000000 00000000 00000000
00000010: 30000000 00007900 60040a00 21046000
00000020: 00000000 00000000 00000000 18000000
00000030: 00080000 891b7340 00000000 00000000
Can someone please confirm if this is correct. If not what should be the correct RCW configuration and how to update the same.
Thanks
已解决! 转到解答。
Hi @devasish
Please refer to the following bit 422-424 in LS1021 Referance Manual section 4.4.6.1 RCW field definitions, please refer to 010 option.
Please follow QCVS_PBL_User_Guide to set RCW parameter according to your requirement.
Thanks
Khushbu Patel
Hi @devasish
Please refer to the following bit 422-424 in LS1021 Referance Manual section 4.4.6.1 RCW field definitions, please refer to 010 option.
Please follow QCVS_PBL_User_Guide to set RCW parameter according to your requirement.
Thanks
Khushbu Patel