LS1021A: PCIe: using multiple MSIs for one EP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021A: PCIe: using multiple MSIs for one EP

1,497 Views
alexanderstein
Contributor II

I need to create a PCIe extension card which must support multiple MSIs, not MSI-X which is not possible on the card. Reading the LS1021A Reference Manual (Rev. 0, 11/2015) 10.2.47 SCFG_PEXMSIIR is the register which must be programmed as the Message Address Register to PCIe EP. The current driver pcie-designware + pci-layerscape does this.

So when a MSI occures the MSI Message Data contains the MSI number, e.g. 0h, 1h, 2h and so on, which is written to SCFG_PEXMSIIR in little-endian. Now reading the register definition IBS, containing the lowest byte of MSI Message Data, ignores the lowest 3 bits at all. MSI requires that MSi numbers are consequtive for one EP. How is this supposed to work if the lowest bits are ignored at all?

Labels (1)
Tags (1)
0 Replies