LS1021 power usage deep sleep

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021 power usage deep sleep

Jump to solution
2,525 Views
dwokke
Contributor II

Hi All,

Does any body have any figures on power usage of the LS1021a in idle, sleep and deep sleep mode?

I realy appreciate your response.

Best regards,

Dennis

Labels (1)
0 Kudos
Reply
1 Solution
2,275 Views
LPP
NXP Employee
NXP Employee

Please, refer to LS1021A Datasheet Chapter 3.4 Power characteristics

Deep sleep 1.0V, 35'C: VDDC 0.15 Watts

Power saving 1.0V, 65'C, 1.0GHz, LPM20: VDDC 0.39 Watts

Power saving 1.0V, 65'C, 1.0GHz, PW15: VDDC 0.05 Watts /core

If you don't have access to this document, create a service request to Freescale support.

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,276 Views
LPP
NXP Employee
NXP Employee

Please, refer to LS1021A Datasheet Chapter 3.4 Power characteristics

Deep sleep 1.0V, 35'C: VDDC 0.15 Watts

Power saving 1.0V, 65'C, 1.0GHz, LPM20: VDDC 0.39 Watts

Power saving 1.0V, 65'C, 1.0GHz, PW15: VDDC 0.05 Watts /core

If you don't have access to this document, create a service request to Freescale support.

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply