LS1021 EDMA single request in u-boot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021 EDMA single request in u-boot

1,844件の閲覧回数
ivanpetrov
Contributor II

Hello.

I am trying to perform a single mem to mem copy in u-boot via edma. Here is my setup for TCD_#0:

int ch = 0;
out_be16(EDMA_BASE + EDMA_TCD_CSR(ch), 0x0);
out_be16(EDMA_BASE + EDMA_TCD_CITER(ch), 0x0);
out_be16(EDMA_BASE + EDMA_TCD_BITER(ch), 0x0);
out_be32(EDMA_BASE + EDMA_TCD_SADDR(ch), 0xA0000000);
out_be32(EDMA_BASE + EDMA_TCD_DADDR(ch), 0xA1000000);
out_be16(EDMA_BASE + EDMA_TCD_ATTR(ch), 0x202);
out_be16(EDMA_BASE + EDMA_TCD_SOFF(ch), 0x4);
out_be32(EDMA_BASE + EDMA_TCD_NBYTES(ch), 1024);
out_be32(EDMA_BASE + EDMA_TCD_SLAST(ch), 0);
out_be16(EDMA_BASE + EDMA_TCD_DOFF(ch), 0x4);
out_be16(EDMA_BASE + EDMA_TCD_CITER(ch), 0x1);
out_be16(EDMA_BASE + EDMA_TCD_BITER(ch), 0x1);
out_be32(EDMA_BASE + EDMA_TCD_DLAST_SGA(ch), 0);

out_be16(EDMA_BASE + EDMA_TCD_CSR(ch), 0x1);

What I was trying to achieve is having 1024 bytes copied from 0xA0000000 to 0xA1000000 in one edma major loop triggered via software. Unfortunately, that didn't work. Nothing was copied and I got an error in DMA_ES (VLD=1; DOE=1; NCE=1), which made no sense to me. And I've also noticed that writing 0x1 to BITER has no effect, as it reads back 0x0.

Is there anything wrong with my setup?

How am I supposed to set CITER=BITER=0x1?

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 返信

1,774件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached eDMA  test example for OCRAM to OCRAM transactions.

0 件の賞賛
返信