Is "Hardware Key Pair Generation" supported by LSDK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is "Hardware Key Pair Generation" supported by LSDK?

Jump to solution
1,383 Views
yutaka_ando
NXP Employee
NXP Employee

The FTF presentation material "FTF-DES-N1858_Security 201 Introduction to QorIQ Trust Architecture_v3.pptx" mentions "Hardware Key Pair Generation" in page 25.  Is this function supported by the current LSDK?  I cannot find any description about this function in LSDKUG.  If not yet, will it be supported in future LSDK?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,284 Views
bpe
NXP Employee
NXP Employee

Yes,  this feature is supported in the current LSDK, see details at the links below:


Hope this helps,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

2 Replies
1,285 Views
bpe
NXP Employee
NXP Employee

Yes,  this feature is supported in the current LSDK, see details at the links below:


Hope this helps,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,284 Views
yutaka_ando
NXP Employee
NXP Employee

Thank you for the answer!

0 Kudos
Reply