LS1020A DDR controller Test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1020A DDR controller Test

3,165 Views
jasonhendrix
Contributor V

How can I test my DDR using the built-in DDR test in the LS1020A DDR controller?

Hi,

I'm trying to run the "automatic memory test" on my DDR by setting up the DDR Ctrl registers.  My first attempt was to set DDR_MTCR[MT_EN] = 1, all other fields in DDR_MTCR were 0.  To my understanding, this should write to all of DDR as specified by CS0_BNDS = 0x008000FF, then read it back.  The test fails immediately, but nothing has been written (and definitely not the entire space).  Why is it failing before even writing?

I also tried setting the test address range, with the same results: (DDR_MTCR[MT_ADDR_EN] = 1, DDR_MT_ST_ADDR  = 0x80000000 and DDR_MT_ENDADDR = 0x81000000.

I did clear the status bit before running each time.

pastedImage_0.png

Labels (1)
0 Kudos
Reply
3 Replies

2,952 Views
addiyi
NXP Employee
NXP Employee

The easiest way to test DDR configuration is to use DDRv tool included in QCVS​.

Adrian

0 Kudos
Reply

2,952 Views
jasonhendrix
Contributor V

Thanks Adrian, we're using that as well.  Does the DDR Test in the ddr controller work?  I would like to see the results of RAM after it writes. 

0 Kudos
Reply

2,952 Views
addiyi
NXP Employee
NXP Employee

Using DDRv, you can choose:

- BIST tests, which are the DDR controller build in tests and will test all the memory using only the controller

- DMA test

- WRC, WO, WZ, which allow you to set the pattern, the size and the start address

- Custom test, which allow you to customize the DDR test

If all the tests from Operational DDR tests are passing, this means your DDR configuration is valid. Starting with this configuration you can run the other validation tests to get the best DDR configuration.

Adrian

0 Kudos
Reply