ARM or Power Architecture

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ARM or Power Architecture

3,278 Views
kimmoli
Contributor I

We have been using PowerPC QUICC processors for some ten years for now, and looking for a CPU for our next project.

On spec-wise LS1021A or P2020 could be a choice, but which one to go with, ARM or Power Architecture core ?

Does NXP continue freescale longevity program?

Is there plans to stop producing new Power Architecture processors, or is the ARM product line just a spin-off test?

Our rough specs are dual-core ~1GHz, >= 2 x1GbE 1588v2, less than 5W

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

2,153 Views
alexander_yakov
NXP Employee
NXP Employee

Below is a link to our recent Roadmap presentation from FTF 2016:

NET-N1863 What's Next for QorIQ - Portfolio and Roadmap.pdf

According to pages 11 and 13, we are currently have roadmaps both Power-based and ARM-based solutions.

I'm not aware about any plans to stop producing new Power Architecture processors, but as you can see the next Power-based processor is not announced for this moment.

Currently, we offer ARM products for Mid-performance and Low-power networking product segments, Power-based solutions for High-performance networking segment.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply