LS1012ARDB K22 Firmware

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1012ARDB K22 Firmware

跳至解决方案
6,278 次查看
jclasquin
Contributor III

Hello,

I'm creating a custom board based on the LS1012ARDB.  I will have the same MK22FX512, connected the same way as on the RDB. 

Where can I find the binary (hex?) files for the bootloader and application that is currently running on the RDB's K22?

I found a file called k22fx512_if_mbed.bin.zip.  I believe that is the application.  I also found a forum post about the bootloader and someone mentioned getting a file called k22fx512_bootloader.bin from someone at NXP.  But I can't actually find that file anywhere.

Can someone please tell me if these are the files I need, and in the case of the bootloader, where I can get it?  I've looked at the mbed source code, but I don't want to change anything and I don't want to rebuild everything.

Thank you,

Joel 

0 项奖励
回复
1 解答
6,191 次查看
ufedor
NXP Employee
NXP Employee

Please refer to the attached binary image and the programming document.

在原帖中查看解决方案

4 回复数
6,192 次查看
ufedor
NXP Employee
NXP Employee

Please refer to the attached binary image and the programming document.

6,192 次查看
jclasquin
Contributor III

One more question.  The programming document is for using a J-Link.  I found that IAR now recommends their own emulator, I-Jet, so I bought one of those.  I thought maybe the programming process would be the same, but when I run JLink.exe I get an error because there is no J-Link connected.  I don't see a similar IJet executable file.

Are there any instructions for using something other than J-Link?  Do I really need to buy another emulator?

Thanks,
Joel 

0 项奖励
回复
6,192 次查看
ufedor
NXP Employee
NXP Employee

We have instructions only for the J-Link.

0 项奖励
回复
6,192 次查看
jclasquin
Contributor III

That's what I needed.  Thanks

0 项奖励
回复