LS1012A SerDes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,693件の閲覧回数
luka_pirnat
Contributor II

Hello,

I'd like to know whether it's possible to have the LS1012 SerDes configured to have both the 2.5G SGMII and RGMII (MAC2). Based on Table 28-2 in the Ref. Manual the SGMII 2.5G and RGMII are mutually exclusive, so it's only possible to have the 1G SGMII when using RGMII. Is this correct?

Also, when configuring one of the SerDes lanes to output the 100-MHz TX_CLK which pins are used? I guess SD1_TX (and not SD1_RX), right? And where should I tie the other pair then (SD1_RX if TX_CLK is output on SD1_TX), to gnd via a pull-down or do I just leave it floating?


Thanks,
Luka

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,568件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes it is correct. All available SGMII 2.5G configurations are presented in the Table 28-2.

Yes SD1_TX pair is used as TX_CLK while SD1_RX pair is an input. It is recommended to connect unused SD1_RX to the GND.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,569件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes it is correct. All available SGMII 2.5G configurations are presented in the Table 28-2.

Yes SD1_TX pair is used as TX_CLK while SD1_RX pair is an input. It is recommended to connect unused SD1_RX to the GND.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------