LS1012A RGMII clocking

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1012A RGMII clocking

跳至解决方案
2,048 次查看
luka_pirnat
Contributor II

Hi there!

We're designing a LS1012A board and we'll be using an RGMII PHY (VSC8531) to connect to the outside world via Ethernet. Now, due to conflict between the CPU Reference Manual and the Design Checklist AN5192 I'd like to make sure it's okay to use two separate clock oscillators for CPU and PHY. Because the ref man only depicts two use cases - the first being using two crystals (CPU and PHY) and the second using a common clock oscillator for both. While in AN5192 the first case is the same and the second shows using a clock osc for CPU and crystal for PHY.

So, is it okay to use two separate clock oscillators/generators for CPU (25MHz) and RGMII PHY (125MHz)? I know the ARDB board does that, but there's also a 0-ohm option left to allow connecting the CPU's ref. clock to the PHY...
The reason for asking this is also a similar problem that existed with SGMII before CPU revision 2.

Thanks,
Luka

标签 (1)
标记 (2)
1 解答
1,941 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

It is Ok to use two separate clock oscillators/generators for CPU (25MHz) and RGMII PHY (125MHz).

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,942 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

It is Ok to use two separate clock oscillators/generators for CPU (25MHz) and RGMII PHY (125MHz).

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------