LS1012A RGMII RTL8211F Ping failed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1012A RGMII RTL8211F Ping failed

跳至解决方案
7,169 次查看
Hugh512
Contributor III

HI, team:

Below is my hardware design, My lsdk version is lsdk 2108

Hugh512_0-1676979033884.png

My dts is as below:

 

&pfe {
	status = "okay";
	#address-cells = <1>;
	#size-cells = <0>;

	pfe_mac0: ethernet@0 {
                compatible = "fsl,pfe-gemac-port";
                #address-cells = <1>;
                #size-cells = <0>;
                reg = <0x0>;    /* GEM_ID */
                fsl,gemac-bus-id = <0x0>; /* BUS_ID */
                /*fsl,gemac-phy-id = <0x2>;  PHY_ID */
                fixed-link = <0 1 1000 0 0>;
                fsl,mdio-mux-val = <0x0>;
                local-mac-address = [ 00 1A 2B 3C 4D 5E ];
                phy-mode = "sgmii";
                fsl,pfe-gemac-if-name = "eth0";
                fsl,pfe-phy-if-flags = <0x0>;
                fsl,pfe-gemac-mode = <0x1B00>; /* GEMAC_SW_CONF | GEMAC_SW_FULL_DUPLEX | GEMAC_SW_SPEED_1G */
                mdio@0 {
                        reg = <0x1>; /* enabled/disabled */
                        fsl,mdio-phy-mask = <0xFFFFFFF9>;
                };
        };

        pfe_mac1: ethernet@1 {
                compatible = "fsl,pfe-gemac-port";
                #address-cells = <1>;
                #size-cells = <0>;
                reg = <0x1>;    /* GEM_ID */
                fsl,gemac-bus-id = < 0x1 >;
                fsl,gemac-phy-id = < 0x1 >;
                fsl,mdio-mux-val = <0x0>;
                local-mac-address = [ 00 AA BB CC DD EE ];
                phy-mode = "rgmii-id";
                fsl,pfe-gemac-if-name = "eth1";
                fsl,pfe-gemac-mode = <0x1B00>;
                mdio@0 {
                        reg = <0x0>; /* enabled/disabled */
                        fsl,mdio-phy-mask = <0xFFFFFFF9>;
                };
        };
};

 

 

After enter command: can't ping 192.168.0.1 successfully. Could you help to check and give suggestions?

 

/ # ifconfig -a
eth0      Link encap:Ethernet  HWaddr 00:1A:2B:3C:4D:5E
          BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

eth1      Link encap:Ethernet  HWaddr 00:AA:BB:CC:DD:EE
          BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

lo        Link encap:Local Loopback
          LOOPBACK  MTU:65536  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

sit0      Link encap:IPv6-in-IPv4
          NOARP  MTU:1480  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

/ # ifconfig eth1 192.168.0.241 up
[   24.200539] pfe 4000000.pfe eth1: pfe_eth_open
[   24.205295] hif_process_client_req: register client_id 1
[   24.210628] pfe_hif_client_register
[   24.214147] pfe 4000000.pfe eth1: pfe_gemac_init
/ # ping 192.168.0.1
PING 192.168.0.1 (192.168.0.1): 56 data bytes
[   61.577760] random: crng init done

 

 

0 项奖励
回复
1 解答
7,154 次查看
Hugh512
Contributor III

 

Dear Chavira:

Thanks, based on your suggestions, I made below modifications and finally can ping gateway success.

diff --git a/drivers/net/phy/realtek.c b/drivers/net/phy/realtek.c
index 746cdfd06578..c0d27537cd54 100644
--- a/drivers/net/phy/realtek.c
+++ b/drivers/net/phy/realtek.c
@@ -749,6 +749,7 @@ module_phy_driver(realtek_drvs);

static const struct mdio_device_id __maybe_unused realtek_tbl[] = {
{ PHY_ID_MATCH_VENDOR(0x001cc800) },
+ { PHY_ID_MATCH_VENDOR(0x001cc916) },
{ }
};

 

before booting into linux, execute command "pfe stop" in uboot. 

 

 

ifconfig eth1 192.168.0.110 up
ping 192.168.0.1
/ # ping 192.168.0.1
PING 192.168.0.1 (192.168.0.1): 56 data bytes
64 bytes from 192.168.0.1: seq=0 ttl=64 time=0.371 ms
64 bytes from 192.168.0.1: seq=1 ttl=64 time=0.343 ms
64 bytes from 192.168.0.1: seq=2 ttl=64 time=0.290 ms
64 bytes from 192.168.0.1: seq=3 ttl=64 time=0.304 ms
64 bytes from 192.168.0.1: seq=4 ttl=64 time=0.325 ms
64 bytes from 192.168.0.1: seq=5 ttl=64 time=0.304 ms
64 bytes from 192.168.0.1: seq=6 ttl=64 time=0.311 ms
64 bytes from 192.168.0.1: seq=7 ttl=64 time=0.324 ms
64 bytes from 192.168.0.1: seq=8 ttl=64 time=0.308 ms

 

 

 

 

 

 

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
7,155 次查看
Hugh512
Contributor III

 

Dear Chavira:

Thanks, based on your suggestions, I made below modifications and finally can ping gateway success.

diff --git a/drivers/net/phy/realtek.c b/drivers/net/phy/realtek.c
index 746cdfd06578..c0d27537cd54 100644
--- a/drivers/net/phy/realtek.c
+++ b/drivers/net/phy/realtek.c
@@ -749,6 +749,7 @@ module_phy_driver(realtek_drvs);

static const struct mdio_device_id __maybe_unused realtek_tbl[] = {
{ PHY_ID_MATCH_VENDOR(0x001cc800) },
+ { PHY_ID_MATCH_VENDOR(0x001cc916) },
{ }
};

 

before booting into linux, execute command "pfe stop" in uboot. 

 

 

ifconfig eth1 192.168.0.110 up
ping 192.168.0.1
/ # ping 192.168.0.1
PING 192.168.0.1 (192.168.0.1): 56 data bytes
64 bytes from 192.168.0.1: seq=0 ttl=64 time=0.371 ms
64 bytes from 192.168.0.1: seq=1 ttl=64 time=0.343 ms
64 bytes from 192.168.0.1: seq=2 ttl=64 time=0.290 ms
64 bytes from 192.168.0.1: seq=3 ttl=64 time=0.304 ms
64 bytes from 192.168.0.1: seq=4 ttl=64 time=0.325 ms
64 bytes from 192.168.0.1: seq=5 ttl=64 time=0.304 ms
64 bytes from 192.168.0.1: seq=6 ttl=64 time=0.311 ms
64 bytes from 192.168.0.1: seq=7 ttl=64 time=0.324 ms
64 bytes from 192.168.0.1: seq=8 ttl=64 time=0.308 ms

 

 

 

 

 

 

 

0 项奖励
回复
7,158 次查看
Chavira
NXP TechSupport
NXP TechSupport

Thank you for contacting NXP support!

I attached a Log of ethernet configuration on Tiny Distro.

the commands are:

ifconfig: you can see the ethernet ports available on the system

ifconfig -a: you can see the ethernet ports of your system

ip link set dev <dev name> up/down : you can set up a device

udhcpc -i <dev name>: you can automatically set up the ip of your network.

the steps that I follow are:
1- Identify the port that you want to use
2- discover the name of your port using the command "ifconfig -a"
3- set up the device with the command "ip link set dev <dev name> up"
4- confirm if the device is ready to set up with "ifconfig"
5- set up the network with the command "udhcpc -i <dev name>" to obtain automatically the IP
5a- If you can set up the IP you can do it with the command "ifconfig <dev> <ip>" for example ifconfig fm1-mac1 10.10.10.10

0 项奖励
回复