LS1012A OCRAM Access

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1012A OCRAM Access

2,868 Views
Gyosun
Contributor III

Hello.

I am using the LS1012A custom board and currently using LSDK1812.
I would like to use OCRAM, but when I try to read it with devmem,
it seems that I don't have the access permission.
I would appreciate it if you could let me know what I should do to read and write to it.

[root@LS1012A ~]# devmem 0x10000000
[  238.273220] Unhandled fault: synchronous external abort (0x92000210) at 0x0000ffff920f1000
Bus error
[root@LS1012A ~]#

Thank you.
Best regards.
Gyosun.

 

0 Kudos
Reply
5 Replies

2,829 Views
khushbur
NXP TechSupport
NXP TechSupport

Hi @Gyosun 

 
I hope you are doing well.
 
OCRAM should not be accessed from user space.
 
It is restricted to Secure World access only by the CSU.
Please refer to Chapter 7 CSU, OCRAM, and MSCM in LS1012ARM
 
One can look into ATF for OCRAM access.
{CSU_CSLX_OCRAM, CSU_S_SUP_RW},
 
here,ocram access is not given to userspace
 
Thanks
Khushbu
0 Kudos
Reply

2,817 Views
Gyosun
Contributor III

Hi Khushbu,

Thank you for your response.

If you could please provide an example of using devmem to set access permissions for CSU OCRAM and read/write to OCRAM, I would greatly appreciate it.

In addition, I tried the following in u-boot, but the CSU_CSL register is not changed.

=> md.l 1510000 8
01510000: ff00ff00 ff00ff00 ff002200 2200ff00 ........."....."
01510010: ff00ff00 ff00ff00 3300ff00 33003300 ...........3.3.3
=> mw.l 1510008 22002200
=> md.l 1510000 8
01510000: ff00ff00 ff00ff00 ff002200 2200ff00 ........."....."
01510010: ff00ff00 ff00ff00 3300ff00 33003300 ...........3.3.3
=> md.l 10000000 8
10000000:"Synchronous Abort" handler, esr 0x96000210
elr: 0000000082058a2c lr : 00000000820589a8 (reloc)
elr: 0000000097ba7a2c lr : 0000000097ba79a8
x0 : 0000000000000009 x1 : 000000000000003a
x2 : 0000000000000020 x3 : 0000000010000000
x4 : 0000000000000000 x5 : 0000000097bbccdd
x6 : 0000000000000004 x7 : 000000000000000f
x8 : 00000000ffffffd0 x9 : 0000000000000008
x10: 0000000000000010 x11: 0000000000000006
x12: 000000000001869f x13: 0000000000000c10
x14: 0000000097b0ceac x15: 0000000000000008
x16: 0000000000000000 x17: 0000000000000000
x18: 0000000097b0ed80 x19: 0000000000000008
x20: 0000000010000000 x21: 0000000010000000
x22: 0000000097bbb778 x23: 0000000000000008
x24: 0000000000000004 x25: 0000000000000004
x26: 0000000000000004 x27: 0000000097b0ccb8
x28: 0000000000000000 x29: 0000000097b0cc30

Resetting CPU ...

### ERROR ### Please RESET the board ###

Thanks,
Gyosun.

 

 

0 Kudos
Reply

2,750 Views
khushbur
NXP TechSupport
NXP TechSupport

 

Hi @Gyosun 

 
Please refer ATF code for OCRAM access.
{CSU_CSLX_OCRAM, CSU_S_SUP_RW},

 

https://github.com/nxp-qoriq/atf/blob/lf_v2.6/plat/nxp/soc-ls1012a/soc.c

enable_layerscape_ns_access(ns_dev, ARRAY_SIZE(ns_dev), NXP_CSU_ADDR);

 

Thanks

Khushbu

0 Kudos
Reply

2,725 Views
Gyosun
Contributor III

Hi khushbur,

 

The code to enable OCRAM was simply written by referring to the code as follows.

void mmap_init(uint8_t **pp_vaddr, uint64_t baddr, uint32_t size)
{
  int fd;
  fd = open("/dev/mem", O_RDWR | O_SYNC);
  *pp_vaddr = (uint8_t *)mmap64(NULL, size, PROT_READ | PROT_WRITE, MAP_SHARED, fd, baddr);
  close(fd);
}

void enable_layerscape_ns_access(void)
{
#define CSU_CSLX_OCRAM (4)
#define CSU_S_SUP_RW (0x22U)

  uint32_t *base;
  uint32_t *reg;
  uint32_t val;
  printf("%s\n", __func__);
  mmap_init((uint8_t **)&base, 0x01510000, 0x1000);

  reg = base + CSU_CSLX_OCRAM / 2U;
  val = be32toh(*(volatile uint32_t*)((uintptr_t)reg));
  if (CSU_CSLX_OCRAM % 2U == 0U) {
    val &= 0x0000ffffU;
    val |= CSU_S_SUP_RW << 16U;
  } else {
    val &= 0xffff0000U;
    val |= CSU_S_SUP_RW;
  }
  *(volatile uint32_t*)(uintptr_t)reg = htobe32(val);
}

However, when reading the value with devmem, the value is not reflected.

[root@LS1012A ]# devmem 0x1510008
0xFF002200
[root@LS1012A ]# ./test
enable_layerscape_ns_access
[root@LS1012A ]# devmem 0x1510008
0xFF002200
[root@LS1012A ]#

What more do we need to do?

Thanks,

Gyosun.

 

0 Kudos
Reply

2,673 Views
khushbur
NXP TechSupport
NXP TechSupport

Hi @Gyosun 

 

You can not update CSU from linux user space.

 
Please refer ATF code for OCRAM access.
{CSU_CSLX_OCRAM, CSU_S_SUP_RW}
 
 
Thanks
Khushbu
0 Kudos
Reply