LS1012A LSDK 21.08 boot failed.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1012A LSDK 21.08 boot failed.

2,348 Views
Gyosun
Contributor III

Hello,

We are porting LSDK 21.08 to a custom board similar to ls1012afrwy.
The SD card was made as follows.

flex-installer -i auto -m ls1012afrwy -d /dev/sdc -r rootfs_lsdk2108_buildroot_devel_arm64.tgz -b boot_LS_arm64_lts_5.10.tgz -p 3P=100M:2G:-1

It seems that the rootfs mount is not working properly during booting.

LSDK2108_boot_fail.txt 

I need help urgently.

Thank you,
Best Regards.
Gyosun.

Labels (1)
0 Kudos
Reply
3 Replies

2,307 Views
Oswalag
NXP TechSupport
NXP TechSupport

ls1012a cannot boot from SD card, you can boot from qspi flash.

0 Kudos
Reply

2,257 Views
Gyosun
Contributor III

Hi Oswalag,

I am currently conducting a boot test using an SD card after QSPI Flash.
The system is displaying the message mentioned above during the SD card boot process and then freezing.

I successfully booted the system by copying the ls1012afrwy_boot.scr file generated in LSDK 18.12 to the SD card boot partition, instead of using the lsdk 21.08 generated file.

Why isn't it working when I try to use the scr file generated in LSDK 21.08?

Thank you.
Best Regards,
Gyosun.

0 Kudos
Reply

2,232 Views
Oswalag
NXP TechSupport
NXP TechSupport

Take a look on the flash layout, you cannot boot from sd  (ls1012), you can use the SD card to deploy only the linux image and ubuntu userland (if it is the case).

Oswalag_0-1696530653134.png

 

0 Kudos
Reply