LS1012A LSDK 21.08 boot failed.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1012A LSDK 21.08 boot failed.

2,355件の閲覧回数
Gyosun
Contributor III

Hello,

We are porting LSDK 21.08 to a custom board similar to ls1012afrwy.
The SD card was made as follows.

flex-installer -i auto -m ls1012afrwy -d /dev/sdc -r rootfs_lsdk2108_buildroot_devel_arm64.tgz -b boot_LS_arm64_lts_5.10.tgz -p 3P=100M:2G:-1

It seems that the rootfs mount is not working properly during booting.

LSDK2108_boot_fail.txt 

I need help urgently.

Thank you,
Best Regards.
Gyosun.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,314件の閲覧回数
Oswalag
NXP TechSupport
NXP TechSupport

ls1012a cannot boot from SD card, you can boot from qspi flash.

0 件の賞賛
返信

2,264件の閲覧回数
Gyosun
Contributor III

Hi Oswalag,

I am currently conducting a boot test using an SD card after QSPI Flash.
The system is displaying the message mentioned above during the SD card boot process and then freezing.

I successfully booted the system by copying the ls1012afrwy_boot.scr file generated in LSDK 18.12 to the SD card boot partition, instead of using the lsdk 21.08 generated file.

Why isn't it working when I try to use the scr file generated in LSDK 21.08?

Thank you.
Best Regards,
Gyosun.

0 件の賞賛
返信

2,239件の閲覧回数
Oswalag
NXP TechSupport
NXP TechSupport

Take a look on the flash layout, you cannot boot from sd  (ls1012), you can use the SD card to deploy only the linux image and ubuntu userland (if it is the case).

Oswalag_0-1696530653134.png

 

0 件の賞賛
返信