LLDP pakcages maintenance problem based on LX2160ARDB?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LLDP pakcages maintenance problem based on LX2160ARDB?

1,315件の閲覧回数
jackho
Contributor IV

Hi,

We use LLDP 5.15.71 based on LX2160ardb platform

About  meta-nxp-deskop layer, it has below describe:

# Note that we have a tight dependency to ubuntu-main
# and that we cannot just install arbitrary Yocto packages to avoid
# rootfs pollution or destruction.

What does this description mean?

How do we add packages with the below parameters on ls-image-main.bb file?

Yocto: IMAGE_INSTALL

Ubuntu : APTGET_EXTRA_PACKAGES

Can I install some package from yocto and some from ubuntu apt?

Is it may cause package conflict, how to avoid it?

 

BR,

Jack

 

0 件の賞賛
返信
1 返信

1,269件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

You are using Ubuntu images, therefore root file system update should be done based on Ubuntu package manager.

IMAGE_INSTALL:append = " ..." should be used for packages that don't have Ubuntu equivalent, which is for example nxp repositories

 APTGET_EXTRA_PACKAGES += "nvmi-cli" should be used for Ubuntu to install nvmi-cli based on apt-get install nvmi-cli.

So, please only use APTGET_EXTRA_PACKAGES to add packages in ls-image-main rootfs.