L3 layer encrypted packets drop in dpdk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

L3 layer encrypted packets drop in dpdk

1,733 Views
rashmikj
Contributor III

I am using dpdk for encrypting IP Packet (IP payload) in L1046ardb Kit. At the receive side , the dpaa driver is dropping the encrypted packet (Not sure whether due to length corruption or checksum corruption as both are encrypted).

How do i disable dpaa not to drop any packets??

I tried the solution mentioned in this thread 

https://community.nxp.com/t5/Layerscape/checksum-disabling-in-dpaa-driver-in-dpdk/m-p/1283323#M8096

but am still not able to receive the packet at the application layer.

 

0 Kudos
Reply
1 Reply

1,724 Views
yipingwang
NXP TechSupport
NXP TechSupport

There are two methods for received L4 checksum error packet from Fman ports,
1. Disable Fman L3/L4 checksum. Unset "DEV_RX_OFFLOAD_CHECKSUM" of "port_conf.rxmode.offloads" to disable L3/L4 checksum for Fman when compile l3fwd application.


2. Receive the checksum error packets to error FQ with the attached patch.

0 Kudos
Reply