DP83822 phy not able to attach (LS1021A) SDK2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DP83822 phy not able to attach (LS1021A) SDK2.0

2,610 Views
winstonjacob
Contributor IV

I am working with LS1021A processor custom board Ethernet configuration, DP83822 phy is used. and here I mentioned my kernel DTS entries. And I attached log and dp83822.c driver which I used in kernel.But the phy is not detected in kernel. I am getting the log like this. Please help me to resolve this issue.

net eth0: could not attach to PHY

net eth1: could not attach to PHY

 

 

DTS entry

======

aliases {
enet2_rgmii_phy = &rgmii_phy1;
enet0_rgmii_phy = &rgmii_phy2;
};

&enet0 {
phy-mode = "rgmii";
fsl,magic-packet;
phy-handle = <&rgmii_phy1>;
phy-connection-type = "rgmii";
status = "okay";
};

&enet2 {
phy-mode = "rgmii";
phy-handle = <&rgmii_phy2>;
fsl,magic-packet;
phy-connection-type = "rgmii";
status = "okay";
};

&mdio0 {
#address-cells = <1>;
#size-cells = <0>;
rgmii_phy1: ethernet-phy@1 {
compatible = "ethernet-phy-ieee802.3-c22";
rx-internal-delay-ps = <1>;
tx-internal-delay-ps = <1>;
reg = <0x1>;
};
rgmii_phy2: ethernet-phy@2 {
compatible = "ethernet-phy-ieee802.3-c22";
rx-internal-delay-ps = <1>;
tx-internal-delay-ps = <1>;
reg = <0x2>;
};
};

0 Kudos
Reply
1 Reply

2,605 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please put dp83822.c in folder drivers/net/phy/, and add the following in drivers/net/phy/Makefile.

obj-$(CONFIG_DP83822_PHY) += dp83822.o

Please enable CONFIG_DP83822_PHY in Linux Kernel configuration file(.config).

In the dts file, please modify compatible = "ethernet-phy-ieee802.3-c22" to compatible = "ti,dp83822", "ethernet-phy-ieee802.3-c22". Please make sure "phy address" is specified correctly in "reg" property.

rgmii_phy1: ethernet-phy@1 {
compatible = "ethernet-phy-ieee802.3-c22"; // compatible = "ti,dp83822", "ethernet-phy-ieee802.3-c22";

rx-internal-delay-ps = <1>;
tx-internal-delay-ps = <1>;
reg = <0x1>;   //phy address
};

0 Kudos
Reply