Issue with executing "decode-dimms" command on LA1224RDB board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue with executing "decode-dimms" command on LA1224RDB board

2,836 次查看
harisankar2001
Contributor I

I'm trying to read Part Number from DIMMS on LA1224RDB through decode-dimms. But Im facing error

"No EEPROM found, the kernel probably does not support your hardware."

Further, I tried to load the ee1004 driver, but still I'm unable to get the information and getting the same error. Looking for help to fix this issue.

0 项奖励
回复
2 回复数

2,772 次查看
khushbur
NXP TechSupport
NXP TechSupport

Hi @harisankar2001 

 

It tells you no eeprom found meaning the existing eeprom driver can't find your SPD, and you're most likely going to need to obtain and load an alternative i2c driver.

 

Thanks

Khushbu

0 项奖励
回复

2,830 次查看
giraffe508
Contributor IV

Hi @harisankar2001 I will write detailed comments,

It seems like you are facing an issue with reading the Part Number from DIMMs on LA1224RDB using the decode-DIMMs command. The error message you are encountering suggests that the kernel might not support your hardware.

First, let's ensure that your kernel has the necessary I2C support enabled. You can check this by running the following command:

 grep I2C /boot/config-$(uname -r) 

If you see the I2C support is enabled (marked with 'y' or 'm'), then proceed to the next step. If not, you will need to recompile your kernel with I2C support enabled.

Next, make sure that the i2c-dev module is loaded. You can load it by running:

 sudo modprobe i2c-dev 

Now, let's check if the ee1004 driver is loaded correctly. Run the following command:

 lsmod | grep ee1004 

If the output shows the ee1004 module, it means the driver is loaded. If not, try loading it again using:

 sudo modprobe ee1004 

Once the ee1004 driver is loaded, try running the decode-DIMMs command again. If you still face the same issue, it's possible that the EEPROM on your DIMMs is not supported by the ee1004 driver. In this case, you might need to look for an alternative driver or method to read the Part Number from your DIMMs.

For more information on using I2C and EEPROM drivers with NXP products, you can refer to the following resources on the NXP community:

0 项奖励
回复