Inquiry Regarding Exporting GPIO Pins on LS1012A Controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inquiry Regarding Exporting GPIO Pins on LS1012A Controller

988 Views
Dhanyalakshmi
Contributor III

Hi team,

I am working with the LS1012A controller and would like to export its sysgpio pins in order to connect some devices on our custom baseboard. However, after reviewing the "Layerscape Linux Distribution POC User Guide," I noticed that it mentions there is no support for the GPIO feature on the LS1012A. Additionally, I built the Yocto-Qoriq SDK from the styhead branch, but in the final root filesystem, I could not find the usual export or unexport files, nor was there a gpio folder in the /sys/class/ directory. I am therefore unsure how to export the sysgpio pins on this platform. Could you please advise on how to proceed?

0 Kudos
Reply
1 Reply

961 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following document about how to use GPIO in Linux filesystem.

https://community.nxp.com/t5/Layerscape-Knowledge-Base/LS1043-GPIO-support-in-Linux-SDK/ta-p/1103689

0 Kudos
Reply