IFC devices testing in Bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IFC devices testing in Bootloader

Jump to solution
3,968 Views
m_syed_ahmed
Contributor III

Hi,

We are working on the LS1021 processor. We had 3 devices (SRAM, NOR Flash, LPC4312) connected on the IFC bus. How to test those devices in the bootloader? For NOR Flash, we were able to validate through the memory read/write command. For SRAM, also we write something in memory and read back to validate that. But, we are stuck in the LPC4312 controller. How to validate that device in the IFC bus?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
3,941 Views
ufedor
NXP Employee
NXP Employee

> Is there a way to calculate IFC timing values for other devices

> like the one excel sheet we had for NOR Flash?

There is no such way.

 

> Also is a memory read/write the only option to validate the IFC bus

Yes.

View solution in original post

0 Kudos
Reply
5 Replies
3,962 Views
ufedor
NXP Employee
NXP Employee

> we are stuck in the LPC4312 controller. How to validate that device in the IFC bus?

The testing has to be determined in accordance with the LPC4312 firmware.

I believe that dedicated test application for the MCU has to be implemented.

0 Kudos
Reply
3,955 Views
m_syed_ahmed
Contributor III

Is there a way to test IFC bus configurations for the corresponding device is fine? I need to validate my IFC Timing and other related parameters.

0 Kudos
Reply
3,951 Views
ufedor
NXP Employee
NXP Employee

The request is not fully clear.

The IFC timings are determined by configured timing parameters.

0 Kudos
Reply
3,945 Views
m_syed_ahmed
Contributor III

Is there a way to calculate IFC timing values for other devices like the one excel sheet we had for NOR Flash?

Also is a memory read/write the only option to validate the IFC bus or do we had dedicated IFC bus test utilities?

0 Kudos
Reply
3,942 Views
ufedor
NXP Employee
NXP Employee

> Is there a way to calculate IFC timing values for other devices

> like the one excel sheet we had for NOR Flash?

There is no such way.

 

> Also is a memory read/write the only option to validate the IFC bus

Yes.

0 Kudos
Reply