IFC devices testing in Bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IFC devices testing in Bootloader

ソリューションへジャンプ
3,982件の閲覧回数
m_syed_ahmed
Contributor III

Hi,

We are working on the LS1021 processor. We had 3 devices (SRAM, NOR Flash, LPC4312) connected on the IFC bus. How to test those devices in the bootloader? For NOR Flash, we were able to validate through the memory read/write command. For SRAM, also we write something in memory and read back to validate that. But, we are stuck in the LPC4312 controller. How to validate that device in the IFC bus?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
3,955件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Is there a way to calculate IFC timing values for other devices

> like the one excel sheet we had for NOR Flash?

There is no such way.

 

> Also is a memory read/write the only option to validate the IFC bus

Yes.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,976件の閲覧回数
ufedor
NXP Employee
NXP Employee

> we are stuck in the LPC4312 controller. How to validate that device in the IFC bus?

The testing has to be determined in accordance with the LPC4312 firmware.

I believe that dedicated test application for the MCU has to be implemented.

0 件の賞賛
返信
3,969件の閲覧回数
m_syed_ahmed
Contributor III

Is there a way to test IFC bus configurations for the corresponding device is fine? I need to validate my IFC Timing and other related parameters.

0 件の賞賛
返信
3,965件の閲覧回数
ufedor
NXP Employee
NXP Employee

The request is not fully clear.

The IFC timings are determined by configured timing parameters.

0 件の賞賛
返信
3,959件の閲覧回数
m_syed_ahmed
Contributor III

Is there a way to calculate IFC timing values for other devices like the one excel sheet we had for NOR Flash?

Also is a memory read/write the only option to validate the IFC bus or do we had dedicated IFC bus test utilities?

0 件の賞賛
返信
3,956件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Is there a way to calculate IFC timing values for other devices

> like the one excel sheet we had for NOR Flash?

There is no such way.

 

> Also is a memory read/write the only option to validate the IFC bus

Yes.

0 件の賞賛
返信