IFC GPCM WE_B usage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IFC GPCM WE_B usage

1,395 Views
benoitmasse
Contributor III

Hi,

In Document Number: LS2088ARM Rev. 1, 09/2020.

In section 17.9 General purpose chip-select machine, in figures 17-46, 17-47, 17-48, 17-49 and 17-50, the WE_B is display as a four bits Bus. But our comprehension is that the WE_B signal is a single bit.

Can you explain why WE_B is display as a 4 bits signal ?

 

Thanks,

 

0 Kudos
Reply
1 Reply

1,386 Views
r8070z
NXP Employee
NXP Employee

These figures do not show WE_B as four bits bus signal. These figures are just sloppy. In the same way  table 17-1 has lost IFC_WE0_B at all.

0 Kudos
Reply