How to use Ethernet functionality

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to use Ethernet functionality

跳至解决方案
1,172 次查看
muaxi8
Contributor V

platform: LX2080a

The Ethernet functionality  depends on the "Ethernet PHY firmware" or "dPAA2-MC" ?

I think it should be depends on the DPAA2, because dPAA2 is extensively described in the manual,

What does Ethernet PHY Firmware  and when should i use it ?  If using DPAA2, then "Ethernet PHY firmware" does not need to program to flash?

muaxi8_0-1628046072122.png

 

0 项奖励
回复
1 解答
1,168 次查看
ufedor
NXP Employee
NXP Employee

The "Ethernet PHY firmware" is required for Inphi IN112525 and is independent of the DPAA2:

https://github.com/NXP/qoriq-firmware-inphi

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,169 次查看
ufedor
NXP Employee
NXP Employee

The "Ethernet PHY firmware" is required for Inphi IN112525 and is independent of the DPAA2:

https://github.com/NXP/qoriq-firmware-inphi

0 项奖励
回复