How to use Ethernet functionality

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use Ethernet functionality

Jump to solution
1,149 Views
muaxi8
Contributor V

platform: LX2080a

The Ethernet functionality  depends on the "Ethernet PHY firmware" or "dPAA2-MC" ?

I think it should be depends on the DPAA2, because dPAA2 is extensively described in the manual,

What does Ethernet PHY Firmware  and when should i use it ?  If using DPAA2, then "Ethernet PHY firmware" does not need to program to flash?

muaxi8_0-1628046072122.png

 

0 Kudos
Reply
1 Solution
1,145 Views
ufedor
NXP Employee
NXP Employee

The "Ethernet PHY firmware" is required for Inphi IN112525 and is independent of the DPAA2:

https://github.com/NXP/qoriq-firmware-inphi

View solution in original post

0 Kudos
Reply
1 Reply
1,146 Views
ufedor
NXP Employee
NXP Employee

The "Ethernet PHY firmware" is required for Inphi IN112525 and is independent of the DPAA2:

https://github.com/NXP/qoriq-firmware-inphi

0 Kudos
Reply