How to handle TVDD pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to handle TVDD pin

Jump to solution
3,154 Views
upartners
Contributor III

In LS1043ARDB, the Pin TVDD(V6) is connected to +TVDD, in our products, we remove the ETHERNET_PHY_10G and do not use any 10G PHY module,the board work without 10G ethnet. We also expect to removing +TVDD power supply chip is U17.
But we do not know how to handle those pins:TVDD(V6),EMI2_MDC(Y6),EMI2_MDIO(W6). Could you please give me some suggestions of handling those pins?

Looking forward to your reply.

Have a great day.

Labels (1)
0 Kudos
Reply
1 Solution
2,326 Views
alexander_yakov
NXP Employee
NXP Employee

According to "LS1043A Design Checklist" (application note AN5012), Table 4, TVDD "must remain powered" if not used.

EMI2_MDC and EMI2_MDIO pins must be tied low through a 2-10 kΩ resistor to ground (GND), or these pins may be configured as a a GPIO and output, and than left floating - this is said in Table 25.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

3 Replies
2,327 Views
alexander_yakov
NXP Employee
NXP Employee

According to "LS1043A Design Checklist" (application note AN5012), Table 4, TVDD "must remain powered" if not used.

EMI2_MDC and EMI2_MDIO pins must be tied low through a 2-10 kΩ resistor to ground (GND), or these pins may be configured as a a GPIO and output, and than left floating - this is said in Table 25.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,326 Views
upartners
Contributor III

Thanks.

I have understood.

Can we tie the TVDD to +1.8V power which supplied by PMIC(U33)? If we can, we can remove the U17.

Looking forward to your reply.

Have a great day.

0 Kudos
Reply
2,326 Views
alexander_yakov
NXP Employee
NXP Employee

If TVDD is not used, you can tie it to any voltage source from the list of supported voltages: 1.2 V, 1.8 V or 2.5 V

Note that even if TVDD is not used, recommended power sequencing for this voltage input must be met.

Please look LS1043A Data Sheet, Section 3.2 "Power sequencing"