Does secure boot use the DDR SPD EEPROM to boot, and if so, how is it used by secure boot?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does secure boot use the DDR SPD EEPROM to boot, and if so, how is it used by secure boot?

1,171 Views
tracysmith
Contributor IV

We are considering removing the DD4 SPD EEPROM from the LS1043ardb and doing secure boot, but we need to understand the implications for doing so for secure boot. 

Does secure boot for SDK 2.0 uboot, or any secure boot software use the DDR initialization or DDR characteristics as part of secure boot for the SPD EEPROM on the LS1043ARDB, or does it use th SPD EEPROM in any way on the LS1043ardb dev boards using SDK 2.0?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

973 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

The secure boot does not care DDR characteristics in the SPD EEPROM.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply