How to create a new Qoriq Configuration Project for LS1024A in CodeWarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to create a new Qoriq Configuration Project for LS1024A in CodeWarrior

1,240 Views
pmccormick
Contributor II

Hello, I am using Code Warrior / QCVS and I am trying to create a new Qoriq Configuration Project for use with the ddr test tool.  On the dialog box entitled "New Qoriq Configuration Project" I am being asked to "Select the processor you would like use" but LS1024A is not one of the choices, I only see LS1020A, LS1021A and LS1022A.  I am using "CodeWarrior Development Studio for QorIQ LS series - ARM V7 ISA Version: 10.0.9 Build Id:170914"  Am I perhaps missing some additional processor support files?  Is there some additional component I need to install?    With the same CodeWarrior install I have successfully used the debugger with the LS1024A, downloaded and stepped through code, programmed flash, etc.

Labels (1)
0 Kudos
Reply
3 Replies

1,023 Views
ufedor
NXP Employee
NXP Employee

LS1024A is not supported by the QCVS.

0 Kudos
Reply

1,023 Views
pmccormick
Contributor II

OK, so is there any plan to support LS1024A in a future version of QCVS?  Or a different nxp product I should be using instead?  I just want to run the ddr test tool...

0 Kudos
Reply

1,023 Views
ufedor
NXP Employee
NXP Employee

Sorry, no plans and no other tool.

0 Kudos
Reply