How to configure/use usb2.0 interface in usb 3.0 port of LS1020A device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to configure/use usb2.0 interface in usb 3.0 port of LS1020A device

ソリューションへジャンプ
2,026件の閲覧回数
infanneraysh
Contributor I

We are using LS1020A processor in our design. USB ports available in the device are 1x USB 3.0 and 1x USB2.0 ULPI. We would like to use USB 2.0 interface alone for internal communication.

Is it ok to use USB_DP and USB_DM signals of the USB 3.0 port as such ?

Is there any configurations needs to be taken care for using USB 2.0 signals from USB 3.0 port ?

Thanks in advance for the support.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,866件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

It is possible to use the LS102A USB 3.0 controller to connect to a USB 2.0 device.

To configure the LS102A USB 3.0 controller into USB 2.0-only mode set USB_GHWPARAMS3[DWC_USB3_SSPHY_INTERFACE]=0.


Have a great day,
Fedor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,867件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

It is possible to use the LS102A USB 3.0 controller to connect to a USB 2.0 device.

To configure the LS102A USB 3.0 controller into USB 2.0-only mode set USB_GHWPARAMS3[DWC_USB3_SSPHY_INTERFACE]=0.


Have a great day,
Fedor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信