How to configure/use usb2.0 interface in usb 3.0 port of LS1020A device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure/use usb2.0 interface in usb 3.0 port of LS1020A device

Jump to solution
2,018 Views
infanneraysh
Contributor I

We are using LS1020A processor in our design. USB ports available in the device are 1x USB 3.0 and 1x USB2.0 ULPI. We would like to use USB 2.0 interface alone for internal communication.

Is it ok to use USB_DP and USB_DM signals of the USB 3.0 port as such ?

Is there any configurations needs to be taken care for using USB 2.0 signals from USB 3.0 port ?

Thanks in advance for the support.

Labels (1)
0 Kudos
Reply
1 Solution
1,858 Views
andrei_skok
NXP Employee
NXP Employee

It is possible to use the LS102A USB 3.0 controller to connect to a USB 2.0 device.

To configure the LS102A USB 3.0 controller into USB 2.0-only mode set USB_GHWPARAMS3[DWC_USB3_SSPHY_INTERFACE]=0.


Have a great day,
Fedor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,859 Views
andrei_skok
NXP Employee
NXP Employee

It is possible to use the LS102A USB 3.0 controller to connect to a USB 2.0 device.

To configure the LS102A USB 3.0 controller into USB 2.0-only mode set USB_GHWPARAMS3[DWC_USB3_SSPHY_INTERFACE]=0.


Have a great day,
Fedor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply