How to assign IPI interrupts to a core other than Core#0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to assign IPI interrupts to a core other than Core#0

3,039 Views
pro-supportengi
NXP Employee
NXP Employee

For SDK 2.0 LS1043ARDB is it possible to isolate a given CPU core from the following IPI interrupts, and if so, how do we isolate CPU0 from the following IPI interrupts:

  • Arch_timer
  • Rescheduling Interrupt
  • Function call interrupt?

root@ls1043ardb:~# echo 498 > /sys/class/gpio/export

root@ls1043ardb:~# echo falling > /sys/class/gpio/gpio498/edge

root@ls1043ardb:~# cat /proc/interrupts

             CPU0         CPU1       CPU2       CPU3

[....]        

66:            0            0          0          0     GIC 106

Level        1740000.jr

67:            0            0          0          0     mpc8xxx-gpio   18

Edge         gpiolib

IPI0:          3226         4833       4237      4170   Recheduling interrupts

IPI1:            17           21         19        23   Function call interrupts

Setting GPIO affinity doesn’t work:

root@ls1043ardb:~# echo 1 > /proc/irq/67/smp_affinity_list

-sh: echo: write error: Input/output error

Setting eMMC interrupt affinity works just fine:

root@ls1043ardb:~# echo 1 > /proc/irq/12/smp_affinity_list

root@ls1043ardb:~# cat /proc/interrupts

             CPU0         CPU1       CPU2       CPU3

[....]        

1:            0            0          0          0     GIC 29

Edge        arch_timer

2:           35475          39336    28975       38803 GIC 30

Edge        arch_timer

11             9           0          0           0    GIC 75 Level    fsl-ifc

12:           3370         14         0           0    GIC 94 Level    mmc0

[...]

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

2,450 Views
Pavel
NXP Employee
NXP Employee

Look at the following pages:

https://access.redhat.com/documentation/en-US/Red_Hat_Enterprise_Linux/6/html/Performance_Tuning_Gui...

and

https://cs.uwaterloo.ca/~brecht/servers/apic/SMP-affinity.txt

and

http://www.thegeekstuff.com/2014/01/linux-interrupts/?utm_source=feedburner

See also the following page from NXP Community:

https://community.nxp.com/thread/301130


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply