How LS1043A boot from emmc?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How LS1043A boot from emmc?

3,437 Views
Hahawell
Contributor III

Hi,expert!

     Our Linux system boots from SD card now, We hope that it boot the system from the EMMC on the PCB board,and SD Card and EMMC use the same SDHC interface.

     We don't find any informations about the operations.

      Otherwise,the debug uart intreface and the ethernet interface work well,and there is a QSPI flash on the PCB board.

      I hope someone can give us some advise.

      Thanks.

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

3,425 Views
Hahawell
Contributor III

How the software download from SD card or ethernet to emmc?

0 Kudos
Reply

3,418 Views
ufedor
NXP Employee
NXP Employee

> How the software download from SD card

It is impossible to simultaneously use SD card and eMMC.

> or ethernet to emmc?

Please refer to the Layerscape Linux SDK Documentation:

https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-DCD3FA8A-CA37-4DCF-B...

section "To program LSDK composite SD firmware image to SD card on LS1043ARDB:"

0 Kudos
Reply

3,433 Views
ufedor
NXP Employee
NXP Employee

> We don't find any informations about the operations.

Which exactly operations?

0 Kudos
Reply

3,425 Views
Hahawell
Contributor III

How the software download from SD card or ethernet to emmc?

Tags (1)
0 Kudos
Reply