GPIO LED support LS1046A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO LED support LS1046A

2,931件の閲覧回数
jhering_ruegen
Contributor II

Hi colleagues,

I am trying to enable LED support via GPIO for our board based on LS1046. In the system I have both mpc8xxx (CONFIG_GPIO_MPC8XXX) based GPIOs and I2C based GPIOs. The LED functionality works for the I2C part e.g.
echo heartbeat > /sys/class/leds/x1p/trigger
but for the LS1046 GPIOs
echo heartbeat > /sys/class/leds/run-g/trigger
not

the same is also with

echo 255 > /sys/class/leds/run-g/brightness


The kernel https://github.com/Freescale/linux-fslc/tree/5.10-2.1.x-imx
attached is the device tree and the kernel configuration file

does anyone have any idea, it looks like the LED support for the qoriq gpio drivers is not working?
Greetings from the island of Rügen
Jörg Hering

0 件の賞賛
返信
1 返信

2,900件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信