Fuse blowing - external power supply

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Fuse blowing - external power supply

877 次查看
OzTheWizard
Contributor III

Hello all,

 

so I'm using Grapeboard which is based on LS1012A. I'm trying to run secure boot and for that purpose I should blow fuses. In order to do that 1.8V should be supplied to SFP_PROG pad. Due to Grapeboard design an external power supply (PS) is needed. This means both PSs, main and external, should have common ground. However, due to unexpected design of barrel PS jack (when plugged disconnects 2 ground points of jack) I ended up in situation using 2 PSs without common ground. Both PS are AC/DC converters.One operatin at 12V and other at 1.8V (with current limitation to 1A). Photo below.

OzTheWizard_1-1628262244527.png

Did I potentially damage the board? 

0 项奖励
回复
1 回复

873 次查看
ufedor
NXP Employee
NXP Employee

> Did I potentially damage the board? 

Not necessarily, but cannot be stated for sure.

0 项奖励
回复