Flex-Builder

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,573件の閲覧回数
notshure
Contributor IV

Hi everyone,

I installed flex-builder following the guide in this document "Layerscape Software Development Kit User Guide, Rev. 20.12, 30 June 2021"

The installation seems to be done well.

When I go to generate LSDK composite firmware with the command:
flex-builder -i mkfw -m ls1043ardb -b sd I get nothing.

It tells me that I am missing the following packages:
1) binfmt-support
2) qemu-user-static

Cattura.PNG

 

I tried installing the missing packages with commands

#binfmt-support:

1) sudo apt-get update -y

2) sudo apt-get install -y binfmt-support

#qemu-user-static:

1) sudo apt-get update -y

2) sudo apt-get install -y qemu-user-static

but I got nothing.

how should I proceed?

0 件の賞賛
返信
1 解決策
2,561件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Ubuntu 20.04 LTS should be installed on the host machine

You need to build LSDK 21.08 under Ubuntu 20.04 host environment.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,562件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Ubuntu 20.04 LTS should be installed on the host machine

You need to build LSDK 21.08 under Ubuntu 20.04 host environment.

0 件の賞賛
返信