Firmware for AQR105 used in LS1088A-RDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Firmware for AQR105 used in LS1088A-RDB

2,458 次查看
carljones
Contributor III

Hello,

We are trying to create a network data storage product based on LS1088ARDB. Our board uses AQR105 similar to what the LS1088ARDB uses. However, we do not have the firmware content of the SPI flash connected to it. Can we request for the firmware used for AQR105 and instructions on how to burn it to the SPI flash via CodeWarrior for ARMv8?

By the way, the thread below is somewhat similar with our case

https://community.nxp.com/thread/493621 

Best,

CJ

0 项奖励
回复
3 回复数

2,215 次查看
Pavel
NXP Employee
NXP Employee

Address request about the AQR105 or AQR107 firmware to Aquantia support:

https://www.aquantia.com/support/

Look at Appendix A of the T1024RDB User Guide:

https://www.nxp.com/webapp/Download?colCode=T1024RDBUG

This document shows requirement for AQR firmware updating.


Have a great day,
Pavel Chubakov

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

2,075 次查看
dswang
Contributor I

Hi Pavel,

Could you please provide the download addresses of the following three files, "added-source-codes-of-API-2.1.0.patch","AQ_API-fix-compile-error-for-API-2.1.0.patch"and "mdio-added-flash-command.patch".

Have a great day,

Dswang

0 项奖励
回复

2,215 次查看
carljones
Contributor III

Thank you for responding and providing links to relevant resources, Pavel.

Will do as advised.

Best,

CJ

0 项奖励
回复