FUID

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FUID

2,479件の閲覧回数
CGW
Contributor I

On the ls1012a "There are two memory-mapped FUIDR registers whose values comprise FUID, the registers are 32-bit RO at addresses 1E8_021C and 1E8_0220. More information on these registers can be found in Trust Architecture Manual." Where are these addresses for the LS1028A?

0 件の賞賛
返信
2 返答(返信)

2,382件の閲覧回数
CGW
Contributor I

Any chance you code provide some code to get access to the FUIDR?

0 件の賞賛
返信

2,461件の閲覧回数
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

The FUIDR is a 64-bit value set (and write protected) with a software readable value. You can use images that
can only pass secure boot on a specific chip.

This FUIDR value is replaced with a process in the LS1028A, such thing does not occur in almost all LayerScape processors.

The reason that the register is replaced with the process is to ensure the protection intended even in the documentation itself.

Thank you for your patience, regards

0 件の賞賛
返信