[LX2160A] DDR4 not working normally

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[LX2160A] DDR4 not working normally

1,487件の閲覧回数
shinhakang
Contributor I

we successfully performed validation and confirmed that there was no fail. However, I created an expert code and applied it to the source, but ddr does not work normally.

When performing clock validation, we saw that appropriate clock delay values were selected in write leveling and read gate training. What register is this value stored in? We can't see the relevant value in the generated ddr_init.c. For ls1046, wrlvl control register exists - (DDR1_DDR_WRLVL_CNTL/2/3) . However, it does not exist on the lx2160a. If the lx2160a doesn't support it, this test seems meaningless. What should we do? Looking forward to your reply.

 

 

shinhakang_1-1677140758493.png

 

Attach log file as below :

log.zip

Thanks

0 件の賞賛
返信
2 返答(返信)

1,471件の閲覧回数
shinhakang
Contributor I

Mrudang,

Then,, how about the attached log. We had passed QVSC validation, but not working normally.

Is there any checking point or idea to resolve.

Thanks,

Shinha.

0 件の賞賛
返信

1,473件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @shinhakang,

LX2160A doesn't require WRLVL_START values. It is done automatically by LX2160A itself. That's the reason the reference manual doesn't have the details.

Regards,
Mrudang

0 件の賞賛
返信